Tool/software:
Hello
I have an LLC DC-DC design with output voltage at 48V and I need to add synchronous rectification controller at the seconder side. I found UCC24624 IC and seems like ok for my design.However as mentioned in the datasheet the VD1 and VD2 pins of UCC24624 can handle up to 230V.If I use center tapped transformer the voltage at each output side will be 48V.
So will the UCC24624 be fine for this design?