Part Number: TIDA-020047
Other Parts Discussed in Thread: AWR2243
Tool/software:
Hi,
While debugging the advanced frame mode, I encountered an issue where the chip failed to start, with the following error code. Please help analyze the cause of this issue:
Error: mmWave Start failed [mmWave Error: -3112 Subsys: 22]. Exception: ./mss/mss_main.c, line 6920.
The location of the error code is:
retVal = rlSensorStart(u8DevMap);
if(retVal != RL_RET_CODE_OK)
{
/* Error: Starting the sensor failed */
* errCode = MMWave_encodeError(MMWave_ErrorLevel_ERROR, MMWAVE_ESENSOR, retVal);
retVal = MINUS_ONE;
goto exit;
}
The configured parameters are as follows:
dfeDataOutputMode 3.0000 channelCfg 15.0000 7.0000 1.0000 15.0000 7.0000 adcCfg 2.0000 1.0000 adcbufCfg -1.0000 0.0000 1.0000 0.0000 1.0000 lowPower 0.0000 0.0000 dataPathClkCfg 1.0000 1.0000 profileCfg 0.0000 78.0000 5.0000 5.0000 17.3800 0.0000 0.0000 11.0000 0.0000 256.0000 22500.0000 0.0000 0.0000 180.0000 profileCfg 1.0000 78.0000 5.0000 5.0000 17.3800 0.0000 0.0000 11.0000 0.0000 256.0000 22500.0000 0.0000 0.0000 30.0000 dataPathConfig 0.0000 1.0000 0.0000 2.0000 64.0000 64.0000 64.0000 0.0000 hsiClockConfig 9.0000 0.0000 hsiLaneConfig 15.0000 1.0000 0.0000 2.0000 0.0000 4.0000 0.0000 5.0000 0.0000 3.0000 0.0000 0.0000 dataFormatConfig 0.0000 1.0000 chirpCfg 0.0000 3.0000 0.0000 0.0000 0.0000 0.0000 0.0000 7.0000 chirpCfg 4.0000 7.0000 1.0000 0.0000 0.0000 0.0000 0.0000 7.0000 advFrameCfg 2.0000 0.0000 0.0000 1.0000 0.0000 2.0000 subFrameCfg 0.0000 0.0000 0.0000 4.0000 32.0000 200.0000 0.0000 1.0000 1.0000 200.0000 subFrameCfg 1.0000 0.0000 4.0000 4.0000 64.0000 200.0000 0.0000 1.0000 1.0000 200.0000 subDataFrameCfg 0.0000 192.0000 128.0000 1.0000 subDataFrameCfg 1.0000 192.0000 256.0000 1.0000 guiMonitor 0.0000 0.0000 0.0000 0.0000 0.0000 0.0000 0.0000 0.0000 0.0000 cfarCfg 1.0000 1.0000 3.0000 16.0000 0.0000 0.0000 1.0000 24.0000 0.0000 7.0000 0.0000 1.0000 cfarCfg 1.0000 0.0000 3.0000 16.0000 0.0000 0.0000 1.0000 25.0000 0.0000 7.0000 0.0000 1.0000 cfarCfg 0.0000 1.0000 3.0000 8.0000 2.0000 0.0000 1.0000 15.0000 0.0000 8.0000 0.0000 1.0000 cfarCfg 0.0000 0.0000 3.0000 16.0000 0.0000 0.0000 1.0000 10.0000 0.0000 4.0000 0.0000 1.0000 compressionCfg -1.0000 1.0000 0.0000 0.5000 8.0000 intfMitigCfg -1.0000 10.0000 10.0000 localMaxCfg -1.0000 5.0000 5.0000 , antennaCalibParams 0.000000 1.000000 0.000000 1.000000 0.000000 1.000000 0.000000 1.000000 0.000000 1.000000 0.000000 1.000000 0.000000 1.000000 0.000000 1.000000 0.000000 1.000000 0.000000 1.000000 0.000000 1.000000 0.000000 1.000000 0.000000 1.000000 0.000000 1.000000 0.000000 1.000000 0.000000 1.000000 0.000000 1.000000 0.000000 1.000000 0.000000 1.000000 0.000000 1.000000 0.000000 1.000000 0.000000 1.000000 0.000000 1.000000 0.000000 1.000000 0.000000 1.000000 0.000000 1.000000 0.000000 1.000000 0.000000 1.000000 0.000000 1.000000 0.000000 1.000000 0.000000 1.000000 0.000000 1.000000 0.000000 1.000000 0.000000 1.000000 0.000000 1.000000 0.000000 1.000000 0.000000 1.000000 0.000000 1.000000 0.000000 1.000000 0.000000 1.000000 0.000000 1.000000 0.000000 1.000000 0.000000 1.000000 0.000000 1.000000 0.000000 1.000000 0.000000 1.000000 0.000000 1.000000 0.000000 1.000000 analogMonitor 0.0000 0.0000 aoaFovCfg -1.0000 -85.0000 85.0000 -30.0000 30.0000 calibData 0.0000 0.0000 0.0000 , appSceneryParams 0.0000 0.0000 1.0000 0.0000 0.0000 -20.0000 20.0000 0.5000 280.0000 -5.0000 15.0000 appGatingParams 8.0000 10.0000 8.0000 4.0000 40.0000 appStateParams 3.0000 2.0000 10.0000 100.0000 10.0000 0.0000 appAllocParams 20.0000 20.0000 1.0000 6.0000 4.0000 20.0000 gtrack 1.0000 1200.0000 35.0000 0.0000 45.0000 0.1522 2.0000 10.0000 0.0000 100.0000 ransac 0.0000 200.0000 1.0000 configDataPort 921600.0000 1.0000