This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-00443: Regarding the issue in implementing the product

Part Number: TIDA-00443


Tool/software:

Hi sir, I have checked with the Controller gate signal generation to the gate driver the controller is generating the signal but while increasing the voltage gradually the duty cycle is not reducing it stays at 95%. Also i have removed the gate driver and checking as it may cause damage if the duty cycle is not reducing. Can you solve this problem or recommend a solution so that i could clear it soon. if i give a 230V input the output voltage is not boosting and it gives only RMS value of 315V DC in output. The boost part is not working. It would be helpful for me if you give me a solution as soon as possible. Thank you sir