This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS546D24S: PSpice for TI Simulation Help

Part Number: TPS546D24S
Other Parts Discussed in Thread: TPS546D24A,

Tool/software:

Hello,

I am having difficulties simulating a two phase design for TPS546D24A in PSpice for TI. We are using a three phase TPS546D24S in our design, but seeing as there is no Spice model for it, we are simulating with the 2-phase "A" variant instead.

I need help setting up the transient simulation. I think I have either a schematic or an initial condition mistake. Can the PSpice schematic be reviewed and assistance provided in simulating the device correctly?

Additional note, I used the TI PSpice model circuit as a starting point, and modified it to match our design as close as we could. I can never get a simulation to work if I start from a blank project. 0.8V_Vout_Schematic.pdf

Thanks,

Ryan