Part Number: TPS548B27
Tool/software:
Hello,
I am not sure I am in the right forum, but here goes.
I am using the TPS548b27 to provide 10 A at 1 V to and FPGA core.
I need to run a transient simulation to confirm performance.
I used WEBENCH to get an initial design
I used this design as a template for a PSPICE circuit. I needed to run the PSPICE simulation with the actual models of the input and output capacitors.
The results were not as expected. See the screenshots below:

Here is the circuit in PSPICE:

I can send the .opj and .DSN files for inspection.
Thanks in advance,
Chuck