Other Parts Discussed in Thread: THS4521
Hi
We are trying to run simulations in PSpice with the model provided for this amplifier, but there is an error when launching the simulation. Here is a screenshot of the circuit:
And the errors encountered are related to the subcircuits in the model, several times:
**** EXPANSION OF SUBCIRCUIT X_U1.X_S2 ****
X_U1.X_S2.S_S2 X_U1.S1_2_DRAIN X_U1.N2663051 X_U1.N2662667
+ X_U1.VEE_BUF X_U1.X_S2._S2 X_U1.X_S2.RS_S2
X_U1.N2662667 X_U1.VEE_BUF 1G
.MODEL X_U1.X_S2._S2 VSWITCH Roff 1e6 Ron 1.0 VH
----------------------------------------------$
ERROR -- 'VH' is not a model parameter name
Is there anything I'm missing? I have seen that people have already made simulations with this model.
Regards
Daniel Contreras Solórzano
Grupo de Tecnología Electrónica
E.T.S.I. Sevilla