Other Parts Discussed in Thread: UCC28019
I'm having a bit of trouble with simulating the UCC28019. I downloaded the latest OrCad Capture and ran the simulation model from the TI site (UCC28019 transient), calculated the necessary values for the components for a 2.2kW PFC which resulted in the following schematic:
I'll put the waveforms in the next post since i can only attach one file at a time.
The original schematic was designed for 350W, I think. But the waveform that resulted is basically the same as the one i posted above. Is there any explanation for this?
Also, when i try to replace the BOOSTCCMDCM component (which I believe is the switching component) with a mosfet, it stops functioning properly (I get very low output and the PFC doesn't do it's job of correcting the source current waveform).
Maybe you can tell me about the limitations of the model...? thank you very much!