This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I just downloaded the SPICE model of TPS40210 : http://www.ti.com/litv/zip/sluc101d
There are three SPICE models of TPS40210 inside the zipped file,
Hi Sheng-wei,
The Startup and Steady State models are used to run time domain simulations. The Average Model is used to run frequency doamin simulations (Bode Plots). The difference between Startup and Steady State model is that in the Steady State model, initial conditions are given to some nodes to make the output start directly in the steady state contition. In the Startup model, VOUT will start from 0V and slowly ramp up to the desired VOUT.
I hope that answers your questions.
Best regards,
Nikhil