This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I'm was looking for 12v to 8v ~2A psu design to use on DesignSpark v4.
The schematic gets imported fine, but PCB just comes in blank.
Looked through readme.txt which came with cad download and found this at the of the document:
WARNING - Component CC0805KRX7R9BB223 is not located on the board, will be removed
WARNING - Component WB_CURRENT_LOAD is not located on the board, will be removed
WARNING - Component WB_BATTERY is not located on the board, will be removed
WARNING - Component CRCW080568K1FKEA is not located on the board, will be removed
WARNING - Component CRCW08058K25FKEA is not located on the board, will be removed
WARNING - Component LMZ14203HTZ/NOPB is not located on the board, will be removed
WARNING - Component CRCW0805137KFKEA is not located on the board, will be removed
WARNING - Component CRCW080532K4FKEA is not located on the board, will be removed
WARNING - Component RR1220P-362-D is not located on the board, will be removed
WARNING - Component WB_GND is not located on the board, will be removed
WARNING - Component CC0805KRX7R9BB472 is not located on the board, will be removed
WARNING - Component C4532X5R1A476M is not located on the board, will be removed
WARNING - Component C3225X5R1E106K is not located on the board, will be removed
Question is if there is a problem with the export, am I missing a step with exporting from website or do these even include pcb designs?
Tried number of designs, but all of them come with the same issue.
Thanks
Andro