Other Parts Discussed in Thread: TPS54625, TPS54525, TPS54622
I have a Webench design for TPS54525(Vinmin=8V, max 13V, Vout 5V Iout=4A) that works ok. I want to reduce Vinmin a bit, say to 6V but I cant even recompile my old design, Vin 7 to 13V. I am recomended to use TPS54625 instead. * Why doesn't Webench accept TPS54525 for this design? In march when I made the first design it was ok! * Is there any Changes made in the Webench tool after releasing new devices that, like in this case, change the recomended parts to use?