webbench limits the freq based on duty cycle limits of the device. but the advertised low load feature (shutting down on a small output over voltage) cannot be exercised this way.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
webbench limits the freq based on duty cycle limits of the device. but the advertised low load feature (shutting down on a small output over voltage) cannot be exercised this way.
Hi,
Sorry for the delay on this I must have missed it come through.
You are right, WEBENCH will not allow you to design using this device in Over Voltage Protection mode (OVP) at full load. If this is something that you really want to do we would recommend consulting the datasheet for design guidance.
Best regards,
Tommy
Hi Koen,
What input/output conditions are you using? (Vin(min), Vin(max), Iout, Ta)
Thanks,
--Hadi