This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I tried to import the spice transient model for LM22671-5.0 in TINA. But it gives me the following error "Invalid Device:$CDNENCSTART. Line #42".
Also I tried simulating the model in Allegro. The basic model gives results but if I change the components then i get incorrect results.
Kindly help me resolve the problem.
Prachi,
The PSpice models for power products are encrypted and can only be used in PSpice version 15.7 or higher. We will add the device to the TINA-TI translation queue. Please note that there are two PSpice models available for the part, a fixed 5.0V output version and the Adjustible version. If you need a different output voltage from 5.0V, please use the ADJ model.
Britt