Hello,
I posted the following question earlier today in the "Clock and Timing" forum, but this may be a better forum to post it:
When I try to open previous LMK04826 WebBench Designs saved under my Login, the WebBench App opens but won't load any designs. It pops up a box that says "Project Not Available".
My designs are a little unusual in that we are trying to simulate the LMK04826 by only using Loop2 with a good 100MHz Reference input. The Loop1 BW is set to 0Hz. The simulations seem to run Ok this way, but maybe this is a problem for re-loading them? Are there any known problems with loading previous designs?
I didn't see any buttons in WebBench for saving the design. Is it saved on the TI server each time the simulation is updated?
Thanks for your help.