This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Prior LMK04826 WebBench Designs won't load from the previous design list saved under my Login (Re-posted)

Hello,

I posted the following question earlier today in the "Clock and Timing" forum, but this may be a better forum to post it:

When I try to open previous LMK04826 WebBench Designs saved under my Login, the WebBench App opens but won't load any designs.  It pops up a box that says "Project Not Available". 

My designs are a little unusual in that we are trying to simulate the LMK04826 by only using Loop2 with a good 100MHz Reference input.  The Loop1 BW is set to 0Hz.  The simulations seem to run Ok this way, but maybe this is a problem for re-loading them?  Are there any known problems with loading previous designs? 

I didn't see any buttons in WebBench for saving the design.  Is it saved on the TI server each time the simulation is updated?

Thanks for your help.