This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD7100 SPICE MODEL FAULTY?

Other Parts Discussed in Thread: UCD7100

Hey everyone,

I've been debugging my spice model for a few days and it seems to me like the UCD7100 model may be faulty. I incorporated it into ltspice and it does trip have the ability to trip when CS is in range of ILIM but not at all in the range that the datasheet says and this is very troubling for my design.

The datasheet says the output is forced low when the CS pin exceeds (ILIM - 25mV) :(see here: 

http://imgur.com/a/FitUq

)

although when i ran the simulation in which i set Ilim to 0.9 volts and slowly increased the CS pin from 0 to 1 Volt i realized it trips at a completely different time. 

(See here: 

http://imgur.com/a/Mi1yg

)

This is the very basic layout i did to test the circuit in lt : (see here: 

http://imgur.com/a/YAj0H

)

and here is a dropbox link to the lt file:

https://www.dropbox.com/sh/9qvuryc4c7na69h/AAAMJEFSN-kY7HBbJrTmhmmTa?dl=0

Any help will be appreciated as this is vital to my design.

Thanks in advance!