This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: TINA-TI or Spice Models
Posted for customer by Alex Scott...
I need support for INA282 PSPICE model, please.
I tried, this morning, to simulate in SPICE the circuitry we have issue with, but did not work.
The simulation problem was related from the PSPICE model of INA282 I downloaded from TI site.
http://www.ti.com/product/INA282/toolssoftware
Simulation Circuit:
Error message:
Picture did not come through - trying again with rich formatting...
Simulation Circuit:
Error message:
Alex,
Sorry I cannot see the picture of your error, but perhaps try the following because I did some kind of error related to the folder read write permission:
1. Download the pspice from the url link you provide
2. After extracting, click right hand click on the properties of the extracted folder, then click make the folder Writable . So if the folder is marked as Read only, unclick that so that the folder and the folders beneath it together with its files are now writable.
On my case, when I try this step, it removes the error.
3. If the step #2 still give you the error, and since I cannot see your picture, try to see the error report and identify which net is dangling (less than 2 connections). Then put the resistor of 1G ohms into that dangling node such as
R1 DANGLINGNODE1 0 1G
R2 DANGLINGNODE2 0 1G
Herman