This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TINA/Spice/UCC28070: ac/dc converter design using UCC28070 controller for 85-265Vrms input and 395Vdc output

Part Number: UCC28070
Other Parts Discussed in Thread: TINA-TI, , UCC28950

Tool/software: TINA-TI or Spice Models

Hi sir,

I was assigned by one project which is basically a AC/DC converter build up with UCC28070 IC Model of TI.From TI portal i got TINA model of this IC and simulated in TINA. its running fine with good results. But there are 3 pins mismatch in TINA application model when compared with the schematic of UCC28070 datasheet. Instead of CDR,RDM and GND pins in the datasheet three other pins used in TINA model i.e. IRIPA,IRIPB and f_khz. For my design require the IC as in the datasheet. For last one month struggling with this problem.But not getting the solution. Finally got your mail id and hope you are the correct person for me to solve this problem. Please suggest me or show me path to get the TINA model of UCC28070 as in the datasheet.
Application model and datasheet attached here.

3286.ucc28070 datasheet.pdf6170.slum328.tsc