Part Number: TPS54160
Tool/software: WEBENCH® Design Tools
Hi,
I want to bring to your notice that there is discrepancy in output voltage ripple obtained from op Vals and steady state simulation of TPS54160.
The design of TPS54160 is in shared link.
To identify which one (op vals or simulation) is appropriate, I have performed calculation based on equation 17 of http://www.ti.com/lit/an/slva630a/slva630a.pdf.
The calculated values are matching well with the op values and the calculations are in attached excel file.
Are they (op vals and simulation) not supposed to give same result?
When I checked with default design of TPS54160, there is no significant difference in values of op vals and simulation. The variation is observed after changing some of BOM components.
Please let me know where the issue is.
Thanks and Regards
Vignesh