Other Parts Discussed in Thread: TINA-TI
Tool/software: WEBENCH® Design Tools
No matter how we try to come at it we cannot get Webench to create an LM5160 based Inverting-Buck-Boost design. On a related note can't seem to get it to generate a fly-buck topology either. For example, if I enter generic design requirements it does not give me a design option that uses the LM5160. If I then check as to why it didn't select the LM5160 this device does not even show up in the list.
Similarly if I try to do it from the LM5160 page the Webench entry does not let me select a negative output. What am I missing? Is the Inverting Buck-boost not supported in Webench for this part? Similar question for fly-buck topology?
The basic requirements are 12V input and -12V @ 500mA output.
Our end goal is to get an export from Webench that we can get into TINA for simulation purposes.
Thank you.