Other Parts Discussed in Thread: TINA-TI,
Tool/software: TINA-TI or Spice Models
pspice models (both encrypted and un-encrypted) for ucc27201A device do not compile
in pspice (version 17)
it appears to be simple syntax error.
pspice reports error "16371" too many characters.
* Model Version: Final 1.10
in voltage source E_U5_E1 the "1.1.75" value in the table does not appear correct.
E_U5_E1 U5_THRISE VSS TABLE { V(VDD, VSS) }
( (8,1.45)(10,1.55)(12,1.65)(14,1.1.75)(16,1.80)(18,1.90)(20,1.95) )
the encrypted model does not compile either. similar error message.
I have corrected the E_U5_E1 and model appears to run.
I did not debug the encrypted model error.
wonder if anyone tested these in pspice?