Other Parts Discussed in Thread: TINA-TI, LMP2012, LMP2011,
Tool/software: TINA-TI or Spice Models
I have recently resimulated a circuit at 3.3V that previously worked at 5V and found it to not simulate properly.
On investigation the issue appears to be that when powered by 3.3V having the LMP2012 amplifiers biased at 3.3V/2 =1.65V does not work (using pspice model LMP2011).
That datasheet indicates specs at VCM=1.35 (half supply) when powered by 2.7V but then list a mush narrower range of −0.3 ≤ VCM ≤ 0.9V when specing CMRR? What is working range?
Is the Pspice model LMP2011 accurate for common mode input voltage range for LMP2012QML-SP at Vsupply=3.3V? Will LMP2012 function normally at 3.3V with VCM=1.65V?
I do have some working engineering boards but need to decide if I should be shifting the bias voltage downward from mid scale if this bias level is unreliable.