Other Parts Discussed in Thread: CDCE62005
The CDCE62005 chip on the EVM has an external reference input at J8. I would like to use a external clock with test equipment (10MHz) to sync up all the signal to the same reference.
The CDCE62005 GUI does not seem to be operational, when I click on it from the main GUI, there is no additional GUI for CDCE62005 that pops up.
Any recommendation for enabling external reference to the CDCE62005?
regards,
Juswanto