This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: TINA-TI or Spice Models
Hi,
The LM8261 SPICE model source E1 is referenced to ground with only 100kohms as series resistance. That makes the simulation model inaccurate with high resistance grounded supplies. SPICE model row:
E1 16 0 17 0 1.0
Should one refer that to PIN 4 (VEE) instead to enable the HRG support?
There's another ground referenced object (RE2 1 Tohm), which doesn't bring that much of problems due to higher resistance. SPICE model row:
RE2 43 0 1.0E12
Can these be fixed in future SPICE model update for this component?