Other Parts Discussed in Thread: TINA-TI
Hello,
It would be nice if SwitcherPro could calculate the output voltage response to a load step under the "What if Analysis" tab.
For example: some DSP consumes about 1A static current and you would analyse what the voltage drop becomes if the processor suddenly needs 0.5A more current, thus a load step of 0.5A. Several factor play of course a role: output capacitance, output capacitor ESR, resistance from PS to load, loop response of PS, etc. Such feature could ease the calculation of the required bulk capacitance to keep the voltage within the right margins if you know the dynamic behaviour of the load.
Is it possible to add such feature to SwitcherPro?
Kind Regards,
Frans