Other Parts Discussed in Thread: TINA-TI
Tool/software: TINA-TI or Spice Models
Hey folks,
after including the .lib file for the Audio amp LM3886 in PSpice by copying the file in the sub folder, opening the file in Spice and selecting auto create new symbol and changing its Value and ModelFile to the right ones i get the same issue all the time.
When i try to run the whole thing it says "Can't resolve .param ibrkv=1m". Unfortunately i got no clue what this could mean and why this happens. I changed nothing in the lib file btw.
I could just figure out that it has to do with this part of the lib file.
I would really appreciate your help.
Kind regards
Fabian Janoth
.SUBCKT lm3886 Vip Vin VDD VSS Vout MUTE IS2 VDD 19 200N IS3 18 VSS -210N Vos 19 20 1M XU7 VDD VSS Vimon PD ILOAD_PD_0 XU2 12 10 11 GNDF PD GBW_SLEW_SE_0 + PARAMS: AOL=115 GBW=8MEG SRP=19.1MEG SRN=19.1MEG IT=1M VON=0.5 ROFF=1M XU3 14 13 PD OUT_CURRENT_CLAMP_PD_0 + PARAMS: RON=0.1 ROFF=100MEG VON=0.5 IMAX=11.5 IMIN=-11.5 XU5 MUTE PD VDD VSS IV110_0 XU4 VDD GNDF 15 16 GNDF PSRR_0 + PARAMS: PSRR=120 FPSRR=8K XU_TF 11 17 GNDF TF_0 + PARAMS: FZ1=10G FZ2=10G FZ3=10G FZ4=10G FZ5=10G FP1=10E6 FP2=10G FP3=10G + FP4=10G XU1 VDD VSS PD IQ_IOFF_0 + PARAMS: VON=0.5 IQQ=50M IOFF=0.5M XD4 VSS 18 IDEAL_DIODE_0 + PARAMS: EMCO=0.01 BRKV=60 IBRKV=1M XD3 18 VDD IDEAL_DIODE_0 + PARAMS: EMCO=0.01 BRKV=60 IBRKV=1M XD2 VSS 19 IDEAL_DIODE_0 + PARAMS: EMCO=0.01 BRKV=60 IBRKV=1M XD1 19 VDD IDEAL_DIODE_0 + PARAMS: EMCO=0.01 BRKV=60 IBRKV=1M XU_GND VDD VSS GNDF GND_FLOAT_0 XU6 13 Vout Vimon AMETER_0 + PARAMS: GAIN=1