This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: TINA-TI or Spice Models
Hi,
I'm looking for a simulation of LMZM33603, input +28V and I want -5V output.
I tried TI's example, but couldn't get the -5V.
Please help.
Thanks,
Vinayak
Hi Vinayak,
PFA the updated .TSC file.
The following modifications were done:
1. The macro file was modified slightly as the earlier model on Webench did not support IBB.
2. All the GND pins(PGND, AGND etc.) need to be connected to Inverting output(-5V in your case).
3. The feedforward capacitor(C4) was too high. I have changed it to 100pF.
4. The feedback resistor(R4) was not in accordance to a VOUT of 5V.
5. Modified analysis parameters to avoid non-convergence.
There is a spike in VOUT at the start of sim due to a capacitor connected between VIN and VOUT(C2). Connect it to ground(0V) if you want to avoid that.
Regards,
Karthik