Tool/software: TINA-TI or Spice Models
My oscilloscope in Tina is not working. I setup a battery hooked up to an voltmeter. I placed my probe on the positive battery terminal. I hook the o-scope probe to the battery terminal. I set the battery up for +5vdc. I go to Analysis -> DC->Table of DC results. I get a table that says I got 5 volts all over the place.
The O-scope is set up for 5volts per vision and 100msec per division. The trigger is set to mode, rising edge, auto with a level of zero. Storage is set to stop. Mode is set to Y/T. X Source is set to VM2 (the only thing it can be set to. Channel is VM2. Coupling is DC and the button is "On".
I get nothing on the o-scope. I even tried auto. Still nothing.