This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: TINA-TI or Spice Models
Hi,
Under Analysis Options, I have enabled "Remember diagram settings". Even after running a plot, setting settings up, closing the plot, re-running, disable the remember settings running again re-enable etc etc etc. You name it. The diagram always opens with all the curves aggregated on one axis.
Any hints?
Aidan
Aidan,
The easiest way to keep curves plotted separately is to add a colon (:) to the end of the name of one of the meters/probes.
That should force all of the curves to plotted on separate axes.
Regards,
John