Other Parts Discussed in Thread: UCC28630, PMP9643
Hi,
Related to the TIDA-00367, is the flyback transformer (T1) design available ?
Thanks,
Manu
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Manu,
Ah this is quite confusing. :-)
I did notice that Wurth has the transformer with them. Actually, we have a transformer manufacturer doing work for us, located here and hence the query related to the transformer design.
Thanks,
Manu
TIDA-00367 Transformer spec.docxHi Manu,
Please find atached a spec sheet for the transformer. This should work for the 100W output you are looiking for. Please take care of minimizing leakage inductance to <4.5uH.
Best Regards,
Ram
Hi Manu,
I have discussed with Ram. There was small typo in the line 8 - "Wind 4 turns of (W2) starting at pin 9 and ending at pin 10". This is W3. This was correctly mentioned in the table.
Thanks,
Manu Balakrishnan