Other Parts Discussed in Thread: LM3488
Tool/software: WEBENCH® Design Tools
Hello Team,
I am in the process of selecting the buck converter for my application. I could find the above mentioned part with my requirements and also i could simulate the same in WebBench tool.
Then i wanted to play around a bit so i exported the model to Tina as .tsc file. Unfortunately the model does not show the behaviour as it is showing in WebBench.
Could you please check the same. I have attached the .tsc file here. Please check.
Specs:
Vin : 8V - 17V
Vout : 18V @ 1Awebench_design_1799836_35.tsc