Part Number: TPS65400
Tool/software: WEBENCH® Design Tools
I am also dsigning the 4 power rails using this TPS65400 chip, but as i want to use webench it don't shows the required output.
My input is 5V, 6A and I want 4 Outputs : 1) 4.1 V, 2) 3.3V, 3) 1.8V and 4) 2.5V .
But when i input my data it shows only 3 outputs and not showing 4.1V output rail.
So, I have a doubt that it will be generated using this chip or not? as I have gone through some reading it can provide output voltage in the range of 0.6V to 90%vin which is 4.5V.
I just want to confirm this before I release it for manufacturing.
Thanks & Regards,
Krutarth