Part Number: TIDA-01022
Other Parts Discussed in Thread: LMK04828, , ADC12DJ3200EVM
the TIDA-01022 uses SYNC_SE to synchronize LMK04828 and the ADC12DJ3200EVM uses LMK04828_SYNC from FPGA. what is the differences between those two approaches.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TIDA-01022
Other Parts Discussed in Thread: LMK04828, , ADC12DJ3200EVM
the TIDA-01022 uses SYNC_SE to synchronize LMK04828 and the ADC12DJ3200EVM uses LMK04828_SYNC from FPGA. what is the differences between those two approaches.
LMK04842 SYNC can be applied using SYNC PIN or via SPI programming
Both TIDA-01022 and ADC12DJ3200EVM has hardware provision given to synchronize LMK04828 but TIDA-01022 SYNC is applied to via SPI programming and LMK04828_SYNC1/2 not used .
JESED SYNC from both TSW14J57 used for ADC1 & ADC2 synchronization using common SYNC generated from SYNC1_SE and SYNC2_SE.