This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/LMZM23601: Can not simulate at Vout = 15 V

Part Number: LMZM23601

Tool/software: WEBENCH® Design Tools

Hi team,

I would like to simulate LMZM23601 under the following conditions,but I can not do it.

Vin=24V,  Vout=15V, Iout(typ)=0.2A, Iout(peak max)=0.7A, Temp=60 degree

I think it is within the recommended operating range described in the data sheet.

Please tell me why the simulation is an error.

Regards,

Takuya Ishikawa