This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/UCC28180: UCC28180

Part Number: UCC28180

Tool/software: WEBENCH® Design Tools

Many of your tools such as, a) Webench  power designer b) UCC 28180 design calculator Revision B (XLS file)gives entirely different component values for the same specification of 1000W PFC at 45kHz. Kindly suggest the recommended tool as soon as possible.

  • Hi Deepak,

    I would suggest Webench power designer, as it is more extensive while calculating the components(but with limited database). Could you please share the input condition you are considering the design for (VinMin, VinMax, Vout, Iout, Temp, Fsw)?

    It would be helpful for us to review, if you could share design calculator with your input condition.

    Best Regards,

    Bhushan    

  • Hi Deepak,

    We did not hear from you for long time. Assuming you are able to resolve the query, I am closing this post. If you have any further queries, please reply here to open the post or create the new thread if this post is locked.

    Best Regards,

    Bhushan