Part Number: LM3481
Tool/software: WEBENCH® Design Tools
I am trying to figure out how the current limiting function works. I am a bit confused since the Webench design is a little different from what the datasheet says. Ultimately I would like to add a trimpot for tuning the current limit if possible. Right now the input voltage is set to 3-4.2V, output voltage 5V, and output current limit to 15A.
In the datasheet, it shows a single resistor- Rsen.
In the Webench design tool, it has an additional resistor. What is Rfilt doing? Is it supposed to be forming a voltage divider? In addition, when I change my desired output current, webench adjusts the value of Rsense. If I wanted to tune the resistance of Rsense in real life, I would need a small footprint SMD power potentiometer, which does not exist. Can Rfilt be made a potentiometer instead since not much power flows across it?