This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/PROCESSOR-SDK-DRA8X-TDA4X: PC simulation doesn't work, shows error

Part Number: PROCESSOR-SDK-DRA8X-TDA4X

Tool/software: WEBENCH® Design Tools

Hello,

I need your help to understand the error that shows up during PC simulation.

I also attach the output report of import tool for our tensorflow model. See attached file. error_report.rtf

The error is:

alex-linux@LinuxV18:/opt/psdk_rtos_auto_j7_06_01_00_15/tidl_j7_01_00_00_00/ti_dl/test$ ./PC_dsp_test_dl_algo.out

Processing config file #0 : testvecs/config/infer/public/tensorflow/tidl_infer_mobileNetv1_0.75_ssd.txt
Error at line:   208 : in file          src/tidl_tb.c, of function : tidl_tb_algCreate
Error Type: TIDL_E_QUANT_STATS_NOT_AVAILABLE            
Error at line:   479 : in file          src/tidl_tb.c, of function : tidlMultiInstanceTest
Error Type: TIDL_E_QUANT_STATS_NOT_AVAILABLE