This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello!
I am trying to control a motor on a car’s sunroof for a project. For this, I am using the TIDA-01421 reference design. I have attached the circuit that I am using.
But I am not able to get any result on an oscilloscope. I have set the sensing probe of the oscilloscope on the timer pin and the ground of the probe with the ground of the motor/power supply. The motor is rated for a maximum stall current of 18A and draws around 2A when running with a power supply. I am not sure what I am doing wrong here since I don’t really have a strong background in electronics. I was hoping that someone could provide some insight.
Thanks in advance!
Gunjan,
Could you post a scope image of the analog signals, starting with the motor current on the right side of R6 w.r.t. ground? That will be a small ripple current on the 6mV (2A x 3 mOhm) voltage. Better if you can capture the signal at U2 pin 5, which is the output of the first gain stage when the motor is running.
I'm assuming the relay should not have any significant impact on the signals.
By the way, the manner in which you have the connections makes it look like you can only drive the motor in one direction. That seems odd for a sunroof.
Hello Clark,
Thanks for your reply. I tried to get a good image on the oscilloscope, but I am not sure if these are the right readings or not...
Signal at right side of R6 w.r.t. ground
Signal at pin 5 of U2 w.r.t. ground
I removed the relays from the circuit in order to reduce uncertainties. I was using two relays, one for forward and the other for backwards motion, but now it's just connected to the power supply directly.
Thanks and regards,
Gunjan
Gunjan
The trace on the sense resistor (R6) looks like typical motor ripple, with 100 mVpp amplitude and frequency about 1.3 kHz. But the output of the INA240 (U2-5) does not show the amplified signal. U2-5 is correctly at half of the 5V supply, but it should also have the amplified ripple. I would concentrate your debug on that stage first. It is acting like it is not connected to the voltage across R6.
-Clark