This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: WEBENCH® Design Tools
Hi,
In TINA I want to simulate the attached design report generated from Webench tool. I want to simulate a Flyback Converter with AC input voltage 220V to 300V and DC Output 24V @ 3A.
Questions :
1. Can I simulate the attached Design in TINA?
2. Is there any sample or example circuit available for my Design AC input voltage 220V to 300 and DC Output 24V @ 3A?WBDesign23.pdf
Hi Shreyas,
As stated in below E2E post as well, Webench do not support electrical simulation for UCC28634. I have forwarded the query for TINA model support to concerned team. We will get back to you soon.
https://e2e.ti.com/support/tools/sim-hw-system-design/f/234/p/897103/3316458#3316458
Best Regards,
Bhushan
Hi Shreyas,
There is no PSPICE model available for the UCC28634, if you want to simulate a flyback circuit there are PSPICE and TINA flyback spice files on the UCC28C42 webpage that would be a useful starting point.
Regards
Peter