Other Parts Discussed in Thread: UCC28710
In bom of PMP9185,the transformer, flyback, 250uH, RLTI-1106 ,I cannot find the specific parameters of transformer,I cannot find RLTI-1106.Can you gei me specific parameters of RLTI-1106. Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
In bom of PMP9185,the transformer, flyback, 250uH, RLTI-1106 ,I cannot find the specific parameters of transformer,I cannot find RLTI-1106.Can you gei me specific parameters of RLTI-1106. Thanks!
RLTI-1106 UPDATE.pdfDear Sir,
attached the data sheet from RENCO,
best regards, Bernd
I want to use the design of PMP9185, but the transformer, flyback, 250uH, RLTI-1106,I can not find it in market,I want to customize the transformer.
I attached the data sheet from RENCO, there is no wire diameter and turns information of transformer. It is necessary to make transformer.
I calculated the designing parameters ,refer to the datasheet of UCC28710.There is on wire diameter and turns in the parameters.
Can you give me wire diameter and turns of RLTI-1106.
Thanks!
Hello Sir,
for building my own high pwr RF xfmrs myself uses Power Stage Designer to figure out RMS current;
having this info I know for WIRE BUNDLES:
AWG22 5A, AWG20 7.5A, AWG18 10A, AWG16 13A, AWG14 17A, AWG12 23A, AWG10 33A, AWG8 46A;
For single wire/open air you could allow more current; at high frequency you have to consider skin effect;
furthermore for bundle please consider proximity effect.
Please check internet for current capabilities of AWG24 and smaller, I do not have this info;
I'm not working on RF power below 1kW.
By knowing the windings ratio you could decide for the number of windings; you need a certain number
to get the flux B to the right range; more flux means more magnetizing losses.
Having calculated the turns you could decide for diameter to achieve best fill factor at bobbin.
For a PSR flyback most important for the windings setup is best coupling aux to secondary to achieve
reasonable load regulation. A sandwich 1/2Pri Aux Sec !/2 Pri is used by myself.
Please do NOT put Aux outside Pri sandwich, does not work for PSR !
(works only for standard flyback using Aux just to power primary ctrl.)
If you never built xfmr in the past I would strongly recommend to get in contact w/ magnetics vendor.
I can't put 30yrs+ of power electronics experience into this small mail, sorry for this.
Hope this helps & best regards, Bernd
Thank you for your reply,it is useful for me.
I did not built xfmr in the past, I will get in contact with magnetics vendor.
Best regards.