This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: WEBENCH® Design Tools
I understand the current TI WEBENCH tool doesn't support PMU devices like TPS65265 now.
Is there any other way we still can use WEBENCH tool to help our design with TPS65265? Can we select a TI power IC with the most suitable/closed IC structure to TPS65265 and then use the WEBENCH tool to design/simulate each of the power bucks of TPS65265 device, respectively for a design reference? Or any other advice?
Thanks!
QH
Hi Qiang Huang,
Yes, the current WEBENCH tool does not support TPS65265. I am not sure on the closest devices to TPS65265 which you can use those to simulate each channel in TPS65265. I will move this post to the right product support forum - so you can get help with suggestions on closest devices, alternate devices and any specific design help.
Best Regards,
Srikanth Pam
Hi, QH
As a best practice, TI recommends to start your design based on TI reference design(EVM board), see below link.
HI, Zhao,
Thank you very much for your quick reply and the EVM info! It is very helpful if the TPS65265-EVM can be used as a design references.
Qiang