This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-01494: Ripple Noise, Power limitation.

Part Number: TIDA-01494


Hi Ti,

We are developing the custom smps board based on the (TIDA-01494 + TIDA0153).

We have some issues.. 

First Case

ripple noise : max 3 Volt. Can you give us some advice..?

Second Case,

the power is limited to the 500W. if the current 18A / 27V is over loaded, the voltage is down to the 24Volt and it's out of order..