This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello there,
I am writing to inquire regarding the testing procedure of tida-01159.
1-Is there any recommended values/specifications for the half bridge circuit? (MOSFETS, Inductor, and capacitors).
2-If the circuit to be tested only to check its basic functionality, can this be done without half bridge circuit? What can be tested without half bridge circuit?
Thank you in advance!
Hi, Mohammad
TIDA-01159 should be able to drive most discrete MOSFET.
You could simulate the MOSFET gate with an equvilant capacitor.
But be attention, you need tie the 'HVGND' with 'GD_HS' together with an jumper, when you testing the output of 'HV_SNODE'.