This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TIDA-00951
Hi,
When we worked at buck mode ,we have noticed that change in the PWM does not change the actual PWM that trigger the gate, there for the d-s is triggerd at ~50%.
i found this thread, which ask Ram the same question but he did not answer it.
can you please clarify it ?
TIDA-00951: A problem about TIDA-00951 48V to 400V Isolated Bidirectional DC/DC Converter Reference Design...
in the photo you can see that PWM trigger of 10% duty cycle correspond to ~50% d-s triggering
yellow and green = 10% duty cycle from the dsp
blue and orange = drain source of q6,q7
Thanks
Michael
Hi, Micheal
have you tried Ramkumar's suggestion, "swap Pin 1& 3 of connector J3 to resolve the problem you are seeing."?
Hi,
yes, but this solution is not refer to the current question.
Thanks
Michael