Can someone help me understand if we utilize a bi-directional step-up converter to adjust the voltage of our battery from 48 volts to 400 volts?
Would this 48v-400v converter work? We have 225 battery cells total so that number does not match up. with theh tech specs. Curious if there are any others options that might work and if we would need to have to UL Certify again. There is a Three Phase Inverter that should work but they sell in EU only.
Three Phase Inverter 48volt in EU market
file:///C:/Users/clarkd/Downloads/Three%20Phase%20Inverter%20Page%203%2048%20Volt%20Battery%20(2).pdf