This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LPSTK-CC1352R: Device doesn't come up on battery power

Part Number: LPSTK-CC1352R

Hello TI-Team,

for a ble demo I want to use the LPSTK-CC1352R as a slave device. If the device is connected via jtag i can flash the multi-sensor example from sdk. Further, after the flash process the device is coming up (only powered via jtag) and i can connect to my master device. If I remove the jtag connection and try to start the lpstk-cc1352R via battery, it doesn't come up. The same problem occure (without battery power) if i remove and reconnect the jtag after flashing. I have to flash the programm again for working.

Before the question is coming up: I already checked the battery for several times and i already reset the device to factory image.

Do you have any idea what the problem could be?

Thanks,

Sebastian