Part Number: CC2640
Other Parts Discussed in Thread: CC2650
Hi All,
I have a custom board with a CC2640F128 chip (it was supposed to be the newest R2 version but due to worldwide shortage..... anyway!)
Then I went to use the SmartRF Studio application and saw it was working correctly (Output status is DONE_OK). I was pretty happy with my board since it has good transmitting power, etc!
Then, I setup a project with the simple_peripheral_cc2650em_app code. If I try to run that code I never reach the SimpleBLEPeripheral_taskFxn function so of course the bluethooth is not working. HOWEVER, If I then go back to the SmartRF Studio, It fails with a Status : IDLE.
If I want the SmartRF Studio to work again, I need to completely Erase my MCU, then try the Studio again and then it works.
So here are the conclusions I have from this:
1) Hardware is working (I can see the broadcasting on my cellphone with good power!)
2) simple_peripheral_cc2650em_app code sets something wrong that makes the MCU unusable afterwards!
3) I can make a led on my board light up with the simple_peripheral_cc2650em_app code.
Do you have any idea what is happening?