This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2642R: How to only remove the two button menus?

Part Number: CC2642R

Hi, 

I want to use the on-chip OAD. 

So I'm using ble5_simple_peripheral_oad_onchip_cc26x2r1lp_persistent_app and simple_peripheral_oad_onchip_CC26X2R1_LAUNCHXL_tirtos_ccs project.

I removed the two buttons menu and display from application project to decrease flash consumption as below link guide.

https://e2e.ti.com/support/wireless-connectivity/bluetooth-group/bluetooth/f/bluetooth-forum/879276/cc2642r-cc2652r-how-to-remove-two-buttons-menu-two_btn_menu-and-display-from-simple_peripheral-project

But I want to use the display function, only remove the two button menus.

I want to check log like the project_zero so I will try to add the UartLog instead of disply_printf.

Because the display_printf seems to require two button menus.

Which one does TI recommend for decreasing memory consumption, display_printf or uartlog?

And then I change IO Capabilities in Only Display Device and disable Two Button Manu - Active Items Only as below.

Does this have problems?

  • Hi,

    This thread is a duplicate of this one. Please avoid double posting.

    I am going to ask you to close this thread. An answer will be provided later on the other thread.

    Thank you for your comprehension.

    Regards,