Part Number: CC2640R2F
I am comparing the power consumption of a custom board and a launchpad for the pin standby example. While the launchpad draws a modes 10µA, my custom board ends up drawing as much as 260µA. This happens with three boards. I was wondering if there is some setting I have missed. Is there a way to verify that the µC was indeed in standby and not just in Idle? Does someone have any similar experiences with current consumption? The reason I am stumped is because there are barely any other components on the board which could drive the consumption so high.
Any ideas or tips are appreciated.