Other Parts Discussed in Thread: CC3200AUDBOOST,
Hi,
I was running the A3DP sink demo, and I found below issues:
1. Every time the device is paired or unpaired by the mobile phone, some pop noise (2 or 3 pop sounds) always occurred in the earphone.
2. When I have two iPhones both paired and connected with the device, I can switch the streaming between two iPhones but there are initially also some pop sounds before it starts to work correctly.
3. When I have two Android phones both paired and connected with the device, the same phenomenon is observed.
4. When I have one iPhone and one Andriod phone both paired and connected with the device, the same phenomenon is observed.
5. When I have one iPhone and another Android phone both paired and connected with the device, some pop sounds occurred when I switch streaming from iPhone to the Andriod phone, but after I switch the streaming back to the iPhone, there is some data corruption (streaming on and off) that will last about 8 seconds before it starts to work correctly. This happens every time.
Does anyone know what causes this issue? Is there some place I can look into regarding this issue?
Regards,
Evan