Hi,
i saw this example on GitHub but i cannot download the "old" SDK 2.30.00.34 version to test the example "peripheral_bidirectional_audio".
I would also like to know if i set it as LINE_IN will it sample 2x 16bit channels at 16kHz , compress and send it to the central device?
Is there an example on the newest SDK or how can i port this example to the latest SDK?
Best regards,
Michael